Yes of course
I have two examples - without additional vendor-specific commands and with.
Example without VS Commands:
1 7 03/16/21 12:39:59.421 +0:00:00.000 BT Logger 1 File 37 5914 2 2 03/16/21 12:39:59.437 +0:00:00.016 BT Logger 1 Assert Level…
Hi David
Sorry about the delay responding. The LMK01020 (LVPECL outputs) can provide 1:4 distribution of the LMX2541 output at 1.5 GHz. Another option would be using the LMK04808 operating at 3 GHz internally dividing down to 1.5 GHz for 4 outputs.…
Other Parts Discussed in Thread: MSP-EXP430FR5969 Hi there,
I am very new to the MSP430 and I am a bit confused by how the 12-bit ADC works. I have an MPC9700 thermistor hooked up to my MSP-EXP430FR5969 Launchpad and I am using the following code example…
Hi Raymond,
thanks for your reply and help.
does the customer want to download the latest SRAM v07 version?
TPS23882_SRAM_Release_Notes_ROM_Advisory_rev_7p0.pdf
Hello, here is the document I referenced. I should have attached it.
7418.Camera_Link.pdf
I am designing a board that will interface with a camera that has full Camera Link capability. I want to bring that data into an FPGA and then transmit the…
Nick,
#1. Customer followed the AM62x Academy Multicore module, page "How to allocate memory", change code and data section in below read frame to MSRAM, keep resource table in DDR0,
put the generated file to Linux filesystem, Can't boot up R5 core…
Other Parts Discussed in Thread: MSP430G2553 Hello
I'm making a C-program for interfacing a AD5933. I have contact with it via i2c, but i'm facing some problems. I've used the I2C example from TI, but with a few modifications. The AD5933 has the 7-bit…
Part Number: AWR1843BOOST Other Parts Discussed in Thread: AWR1843 HI,
I am referring the "TI mmWave Radar sensor RF PCB Design, Manufacturing and Validation Guide" document for the RF PCB design. In this document it is mention that the thickness of…
Part Number: AM5726 Other Parts Discussed in Thread: SYSCONFIG
Hi, I am trying to boot a custom board with an AM5726 SoC. I'm told the design of the board has influences from the IDK, however the PMIC is not directly connected to the AM5726, as it has…
Part Number: TCA8418 Tool/software: Hello!
I have encountered a bug where, in between a correct key press and key release event, I would get a false key press and key release. This does not always happen, and when it does, it is very brief. Not only…