Hi Tess,
I don't have one with single DDR3 DRAM. Here is the one with single DDR2 for your reference.
Regards,
Weidong
TIDA080004_formatter_schematic.pdf
Hello Manikanta:
Yes, we tried: each has a challenge.
UCC256404 requires huge inductance values and Vcr is also very high. See attached LLC worksheet- errors I do not have access to fix.
On the other hand, 28740 flyback will generate Vfly too high…
I have attached document that describes the correct installation procedure and process for connecting to the gauge to communicate. See if you can get the EVSW to work with this guide. If not, there may be an issue with the chip, the EV2300, or any of…
Martin,
As I mentioned previously, we do not have such information. Our Modules are for commercial use therefore those tests are not performed.
I would recommend going to ti.com, click on top left corner "Applications" and select "Aerospace & defense…
Hi Ulrich I have changed the shunt from 14mR to 10mR. The input current is now cleanly sinusoidal. Many thanks for the great support. I have checked the calculator again. it still says 14mR (see excel). Should I pay attention to something if I simply…
Hi,
we do not have the file in Eagle.
Following you can find the pick and place file.
Thanks
Best Regards
Riccardo
TIDA-010938 DC-DCE1_PnP.xls TIDA-010938 AC-DCE1_PnP.csv
OK,
But I used AMC1301 because that I follow TI design SPEC "Reference Design for Reinforced Isolation Three-Phase Inverter With Current, Voltage, and Temp Protection"
ti isolation design.pdf