Part Number: TMS320F28335 Hi
I looked up the Solar Explorer Development Kit TMDSSOLARCEXPKIT, TMDSSOLARPEXPKIT fot development in the TI site and Google. But it is not available.
So i wonder the Solar Explorer Development Kit is discontinued.
And if so…
Part Number: TMDSSOLARPEXPKIT
Tool/software: Code Composer Studio
I am using Sine analyzer with power (SINEANALYZER_DIFF_wPWR_IQ). It works very well with voltage RMS, but I have problem with get appropriate value from current RMS. The value fluctuate…
Part Number: TMDSSOLARPEXPKIT I try to work multiple inverters in parallel sharing one load. I am using the inverter stage from the TMDSSOLARPEXPKIT At first, I was thinking, that I can generate waveform from one inverter, and with use of the PLL synchronize…
Part Number: TMDSSOLARPEXPKIT I made hardware changes to inverter stage from TMDSSOLARPEXPKIT so it can work with lower current that is <100mA. I changed some resistors responsible for gain of the op-amps. The changes I made was:
R15, R18, R19,R20 from…
Part Number: TMDSSOLARPEXPKIT I am using the module SINEANALYZER_DIFF_wPWR_IQ with TMDSSOLARPEXPKIT.
When I try to add initialization, the output frequency is changed.
After adding
sineanalyzer_diff_wpwr1.SampleFreq = 40000;
sineanalyzer_diff_wpwr1.Threshold…
Part Number: TMDSSOLARPEXPKIT Good morning,
I want to adapt TMDSSOLARPEXPKIT to load around 1k Ohm. I switched frequency to 40kHz from 20kHz, also adapt new SPLL v1.2 instead of 1.0. I had trouble with the current measure in inverter leg but I found out…
Part Number: TMDSSOLARPEXPKIT On the schematic, I see that some resistors on the Inverter stage have diffrent value than on board.
I try to build just inverter module standalone and do not know which value I should use and why there is that difference…
Part Number: TMDSSOLARPEXPKIT I have to replace my gate driver on TMDSSOLARPEXPKIT, because I burned down the original. This is U3 on inverter stage and after replacement when I ran project in Build 1 I receive that gaps in PWM signals:
It happens only…
Part Number: TMDSSOLARPEXPKIT Tool/software: WEBENCH® Design Tools Dear TI Community Greeting!!
I want to know how to change the V-I Characteristics of PV Emulator in Solar Explorer Kit. When I will be able to change it, I will be able to have to achieve…