Part Number: UCD3138FW_LLC Tool/software: TI C/C++ Compiler Hi TI
I had bought TI demo board UCD3138LLCEVM-028,
but there doesnt have F.W support on TI Web as others demo board.
may I get this F.W source code for further study??
I am designing a digital controller for the LLC resonant converter using the evaluation module UCD3138LLCEVM-028 alongside the control card UCD3138LLCEVM-030. How can i find the values of the resonant circuit parameters, Lr, Lm and Cr and so on as the…
Other Parts Discussed in Thread: UCD3138 Hi,
My company has bought UCD3138LLCEVM-028 evaluation module. Should we register it in order to get access to C source code for the module.
Part Number: UCD3138ALLCEVM150 Other Parts Discussed in Thread: UCD3138A , UCD3138 Tool/software: Code Composer Studio Hi,
We recently got the EVM UCD3138ALLCEVM150 for digital LLC evaluation. This EVM has UCD3138A micro and UCC7138 chip for synchronous…
Part Number: UCD3138 Tool/software: Code Composer Studio In the UCD3138LLCEVM-028 code, in main.c there is a code copied below, what does it mean?
//Check to see if FAULT2 is pulled high and FAULT0 is pulled low. //If they are go to ROM. if (MiscAnalogRegs…
None of the EVMs are 100% match your requirements, but the most close one is UCD3138LLCEVM-028. It use two PWMs, each with 50% duty, no overlap, with frequency modulation. It has unused PWMs which can be used to control the daughter card.
Regards,
B…
Other Parts Discussed in Thread: UCD3138OL64EVM-031 I try read LLC firmware(UCD3138LLCEVM-028).
In configuration_functions.c .
I don't understand what pmbus_dcdc_config[0].deal_time_X .
Uint32 dead_time_1_local;
Uint32 dead_time_3_local;
Uint32 dead_time_4_local;…
HI Brandon,
I have purchased the evaluation UCD3138LLCEVM-028 but I have no sample code,
So I can't understand very well , especially the configuration of register.
Could you please send me the source code for UCD3138PFCEVM-029 and UCD3138LLCEVM-028…
Other Parts Discussed in Thread: UCD3138PSFBEVM-027 , UCD3138PFCEVM-026 Hi Sir
I bought ucd3138pfcevm-026, ucd3138psfbevm-027, ucd3138llcevm-028 from mouser.com
Could I get these source codes of EVMs.
my email: cshuenko@gmail.com
regard.
Dear Brandon,
I am a power supply engineer and now i am using the ucd3138LLCEVM-028.So I really need source code.Could you send the source code to me?My email:sunwenyang518@163.com
Thank you very much