Part Number: ADC128S102 Hello,
I want to configure continuous conversion mode on ADC128s102 using Raspberry pi to achieve 1 MSPS throughput when using single channel and 125 KSPS per channel when using all 8 channels, can anyone suggest me how to configure…
Other Parts Discussed in Thread: CC2530 , CC2531 I am working on a project where Raspberry Pi is the ZigBee coordinator and TIVA-C (123 or 129) launchpad are router/end-device.
I think on the RPI, we can use a CC2531 usb dongle . Is there any CC2530…
Part Number: TLV1504 Tool/software: Linux TLV1504 ADC IC,:
Setting : FS always high , CPOL = 0, CPHA = 0 and speed = 20MHz
But I read the data first byte always 0x10 and the other byte is zero
Does anyone have a suggest with my settings?
Part Number: TLV1504 Tool/software: Linux TLV1504 ADC IC,:
Setting : FS always high , CPOL = 0, CPHA = 0 and speed = 20MHz
But I read the data first byte always 0x10 and the other byte is zero
Does everyone have a suggest with my settings?
Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: CC1310 Hello,
I got a project for which i was tasked to build a drone that would use object detection to identify people. I'm planning on using the cc1310 to transmit pictures from the drone…
Other Parts Discussed in Thread: FDC2214EVM Hi, is there any way to interface the FDC2214EVM sensor with a Linux-based system (since the GUI is only available on Windows) or connect it to a Raspberry Pi and receive data? Is there code available for Linux…
Tool/software: Linux I have successfully butchered a USB WiFi dongle and attached it to my raspberry pi zero by attaching the USB connections on the dongle to the USB test pads on the raspberry PI
I thought that TI might have a product / design which…
Hi ,
I want to connect two CC2650 with my raspberry pi, I am using GATT client in my raspberry pi.
Can any body help me into writing GATT client for multiple server interfacing simultaneously.
Please help.
Thank you
Other Parts Discussed in Thread: AM26LV32E Hello there :)
As I am really new to this topic, I hope I can get some help here ;)
What I am looking for, is a RS422 Receiver with two differential line pairs, which returns a 3,3 V TTL signal for my raspberry…
Part Number: CC2530
On this system (old 1.0.1 gateway) the INVALID_PARAMETER issue also appears, and I was contacted for remote support of one of the demo systems.
In order to check if the connection was actually used by the gateway, I tried to access…