Part Number: LMH32401
Other Parts Discussed in Thread: LMH5401, LMH6401
Hello Team
There is a application question about LMH32401. run the simulation in TINA, looks like work well.
1. if Vocm pin not used. could I add a RC(50Ohm+0.1uF) to do the termination.
2. if Vod pin not used. could I add a RC(50Ohm+0.1uF) to do the termination.
is there any potential risk when real situation? the post amplifier will be high-speed fully differential amplifier. the input common voltage is around 0V.