Part Number: OPA857-DIE
Other Parts Discussed in Thread: OPA857, , OPA855, LMH32401, OPA858, OPA859, OPA856
Hello,
I was wondering if there are any experimental/test data about this device?
I would expect the input capacitance to be affected by the packaging of the OPA857, therefore I would expect a lower capacity and broader bandwidth for the OPA857-DIE compared to the OPA857.
And also as a consequence, if it's been tested with lower photodiode capacitance than 1.5pF. This is because the photodiodes I intend to use will have a capacitance of 0.3pF.
Kind regards,
Francesco