Part Number: LMC6035
Folks,
I have a question regarding the maximum sink/source current or the LMC6035.
The Abs Max table suggests that the maximum output current is +/-18mA with 30mA as an acceptable short-term value (note 5).

Though the typical output current as shown in Figure 4 and Figure 6 suggests that 100mA is possible:

Couple of questions:
1. What is the maximum allowed output current?
2. Can you quantify the amount of time that would be considered "long term" in the abs max table?
Don