Part Number: PGA309
Hi
If PRG is configured as one-wire UART interface, what will be the voltage and current levels of PRG pin?
Regards
Dewanshi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PGA309
Hi
If PRG is configured as one-wire UART interface, what will be the voltage and current levels of PRG pin?
Regards
Dewanshi
Hi Dewanshi,
The PGA309 datasheet specifies the PRG logic input levels:
It accepts a 0.2*VSD (maximum) for logic input low, and 0.7*VSD (minimum) for logic input high; where VSD is the digital supply voltage. The allowed digital supply voltage range is 2.7V to 5.5V.
The PRG Output is an open drain, and specifies a low level of 0.4V maximum while sinking 5mA.
Thank you and Regards,
Luis

HI Dewanshi,
The PGA309 User Guide provides a detailed discussion about the PGA309 PRG pin configuration and circuit configurations/protection.
Section 4.10 of the PGA309 User Guide (p.88) documents the One-Wire Operation with PRG Connected to VOUT. Pages 88-90 discuss the circuit, PGA309 register configuration that allows the One-Wire interface pin (PRG) to be tied directly to the PGA309 output pin (VOUT).
Section 4.11 of the PGA309 User Guide (p.91) discusses four-wire sensor modules, where the PRG is connected separately from VOUT. Pages 91-93 discuss the PRG ESD and overstress protection, and Figure 4-21 shows an example of external protection circuits EMI/RFI filtering and ESD protection for the PRG pin on the four-wire module.
Thank you and Regards,
Luis