Part Number: OPA192
Hi,
1. Kindly let me know the Value of maximum current consumption of OPA192 @VCC=3.3V and VSS=-3.3V.
2. I want to generate -3.3V from 5V supply. so how much output current i need to consider?
3. Aslo suggest me any IC having 5 to -3.3V suitable for OPA192.
4. Iam using Rsense =10R for high and low side sense(120ma and 24mA). Am i able to sense voltage by using this resistor?
5. Iam sensing 5mV also by using this opamp(gain maximum i can set is 1.8)Is it possible to sense?
Thanks
Monisha OM