Part Number: OPA191
Hi team,
As datasheet Absolute Maximum Rating description.Signal input pins (Differential ) is (V+) – (V–) + 0.2 V.
If the V+,V- supply are +-3.3V. when input signal is IN+ is -5V, IN- is 0V. this situation will damage the device? or any impact?
when this condition and just limit input current <10mA. Is ok or not? thanks