This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA240: alternative with smaller package size

Part Number: INA240


Hi Team,

INA240A1 fits all customers requirements but one, the package size.
Could you please recommend a smaller alternative?

Application: current sesne for position control
Common mode voltage >=60V
R_shunt: 27mOhm
Gain: 20V/V
nominal bridge voltage: 36V up to 45V

BR,
Stefan