Part Number: LM2903B-Q1
Could you please provide comparison table of LM2903BQDRQ1 vs LM2903AVQDRQ1.
Regards,
kura
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM2903B-Q1
Could you please provide comparison table of LM2903BQDRQ1 vs LM2903AVQDRQ1.
Regards,
kura
Kura
are you looking for more than the comparison table at the bottom of the datasheet?
Chuck
Like this?
| OPN | LM2903BQDRQ1 | LM2903AVQDRQ1 |
| Manufacturer | TI | TI |
| Pinout | OPAMP_DUAL | OPAMP_DUAL |
| Channels | 2 | 2 |
| Pkg | D8 | D8 |
| Tmin | -40 | -40 |
| Tmax | 125 | 125 |
| VccMin | 2 | 2 |
| VccMax | 36 | 32 |
| Tresp (us) | 1.000 | 1.300 |
| Is Max Ch (uA) | 0.3 | 0.5 |
| InRange | To V- | To V- |
| OutRange | OC | OC |
| VosTyp (mV) | 0.37 | 1 |
| VosRmMax (mV) | 2.5 | 2 |
| IbiasTyp (nA) | 3.5 | 25 |
| Auto Qual | Q1 | Q1 |
| Datasheet | LM2903-Q1 | LM2903-Q1 |