Part Number: TLV4172
I am trying using integration circuit to detect the variable current which is generated by optical sensitive sensor R3(the sensor resistance is around 500K Ohm), I have measured the sensor and confirmed the sensor functions well (the sensor resistance is around 350K Ohm at 45℃ and the sensor resistance is around 600K Ohm at 22℃) and also simulation result looks fine too. But in real circuit the output keeps saturated, which should keep changing with variable thermal, please let me know any issues.
Many thanks in advance.