Part Number: TLV2186
Hi,
I have a question regarding the max. output current of the op amp TLV2186.
According to the datasheet, "Short-circuit to ground: continuous", it is safe to short the op amp output to ground.
But what about shorting the output e.g. to the positive supply rail?
Consider this case: the op amp is supplied by single-supply 12V and configured as voltage follower. The input is 0V, but the op amp output is connected to +12V.
The op amp will try to output 0V, but due to the short-circuit, it can't and a current will flow into the opamp output.
Will the current still be limited, or would this destroy the op amp?
Under "electrical characteristics", the short circuit output current is specified as +/-20mA (positive and negative) , so can I assume that the output is also protected wen sinking and not sourcing current?
Thanks in advance for your help!
Regards,
Marcel