Part Number: TLV3502
Other Parts Discussed in Thread: TLV3201,
Is there an evaluation board for TLV3502 and TLV3201? I don't see one on the product folder page. If not, is there a coupon board?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello TJ,
There are not any specific boards for these devices, they are pretty generic and simple and easy to prototype.
We do have SMT to DIP adapter boards:
There are also similar, lower cost SMT to DIP adapters kits available from Mouser, Digikey, Amazon and eBay.
Though I will warn you that due to the TLV3502's speed, there needs to be a 0.1uF ceramic bypass cap mounted directly between the supply pins on the adapter board, and keep the I/O leads short.