Other Parts Discussed in Thread: INA200, INA282
Dear All
Using two INA200 to sense current in HIGH and LOW side of a load. The system power supply is 28VDC. Current sense resistors are 0.01 Ohm each. Sensed current is 550mA. Filter resistors are 100 Ohms each in series with inverting and non-inverting inputs.
Given the the published characteristics the calculated ideal voltage output as measured at pin 2 of INA200 should be 20*0.55*0.01 = 0.11 volt. The actual measured voltages, however, are:
for the high side = 0.0961 volt
for the low side = 0.1086 volt
Note that high side INA200 is measuring in the presence of 28 VDC common mode voltage whereas low side INA200 is within few millivolts of ground common mode voltage.
Given the above scenario can anybody shed some light on the measured output errors as given above, particularly the high side one.
Regards
i.k.