Other Parts Discussed in Thread: TM4C1233H6PZ, INA226
Using of 96 x INA228 Power monitors with the TM4C1233H6PZ Microcontroller
There are 6 x I2C buses on the Microcontroller. Connecting 16 INA228 power monitors per I2C bus should be possible
Measurements from the Power Monitors are to be transmitted on a USB 2.0 bus to host PC.
Two Questions:
1- Can the Microcontroller handle 96 loads on the I2C buses? (assume 400KHz I2C clock)
2- What would be the maximum number of times each power monitor device can be sampled every second ?