Part Number: LMH6554
Hi
I am confused about this figure in the datasheet, and I want to make sure I understand it so as to ensure it is suitable to my application.
VOD is shown going as high as ~1.35 V and then clipping. Is this plot showing the output as single-ended to ground? It's labelled as "Vod", but other plots show the differential output voltage to reach as high as +2V and -2V (see figure 7).

If that's true, is the gain of the plot above Av=5?