Other Parts Discussed in Thread: OPA847
Hello TI Member :
I am trying to use an oscilloscope to measure the PSRR of OPA2836, but I am not sure whether the test environment can verify it, could you help me to check whether my test setup and method are correct? Thank you!
1. set the OPA2836 as an unity- gain buffer
2. let VS+ = AVDD = 5.0V, VS- = AVSS = 0V, VIN1+ = AVDD/2 = 2.5V , VIN2+ = AVSS = 0V , Rloading = 2.2 kohm
3. add AVDD with a noisy source ( 1 KHz sin wave, Vpp = 500 mV )
4. let the probe tie to ground and record the wavefom of probe ( I think this can be the noise floor caused by probe, so I need to exclude it, you can see the scope capture that named " VOUT_Floor " )
5. use a 1:1 probe to measure VOUT1 's ripple
6. use the math function to get VOUT1 's ripple which is named " VOUT - floor "
7. record the value peak-peak of ripple
8. PSRR = 20 Log ( 501.30 / 1.046 ) ~ = 53.6113 dB
Thank you for your any suggestion!
B.R
Chen