Other Parts Discussed in Thread: OPA855
Hi all,
I am adapting this EVM to be a TIA with Rf = 30k.
I have connected a high speed balanced detector with diode capacitance about 260fF capacitance (520fF total) to the -VE input directly at the junction pad of R2/R4.
R4 of course has been removed.
The +VE input is unchanged from EVM default.
Running OPA855 at +- 2.5V.
Have tried using nothing and also 100fF as my Cf but in both instances I am seeing a strong oscillation around 8MHz.
This is strange, since if there were stability problems I would expect them at much higher frequencies.
Any ideas to solve this are welcome.
David