This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA333AIDBVR

Other Parts Discussed in Thread: ADS8881

THE DESIGN USING THESE OP AMPS IS TO GENERATE A REFERNCE VOLTAGE FOR THE ADC "ADS8881IDGS". THE INPUT VOLTAGE IS SET TO 5.5V TO THE OP AMP ANAD HAS TO GENERAT A ADC_REF VOLTAGE OF 4.5V ACCORDING TO THE DATASHEETS.

  • Hi Aswathy,

    why aren't you following the recommendation given in figure 65 of datasheet of ADS8881? Your R152 is way too big and your C169 is way too little.

    Kai

  • Hi Aswathy,

    As Kai has mentioned, the value of the R152 resistor needs to be a much smaller 0.2Ω, and the proper REF bypass capacitor needs to be 10-μF as recommended on the ADS8881 datasheet

    The 10-μF REF bypass capacitor along with the 0.2Ω resistor need to be placed in very close proximity to the ADS8881 REF pin.  Choose a 10-μF, X7R-grade, 0805-size, ceramic capacitor with at least a 10-V rating for good performance. Below is the circuit recommended in the ADS8881 datasheet.  Also, please refer to Figure 77 of the ADS8881 datasheet for a board layout example showing the optimal placement of the 10-μF bypass capacitor and 0.2Ω  resistor in close proximity to the REF input of the ADS8881.

    Thank you and Regards,

    Luis