Hi All,
I would like to ask a question on OPA357AIDBVT power.
What is the proper power supply for OPA357AIDBVT?

The upper of the following images is from SpectrumDigital’s DaVinci EVM which uses three OPA357AIDBVRG4 for its video output, while the lower is another EVM that uses three OPA357AIDBVT.
The question is on how should power supply be filtered? In addition to the components found in the lower image, SpectrumDigital’s schematic still has:
|
C255 |
0.01uF |
|
L16 |
BLM41P750SPT In total it has two BLM41P750SPT now |
|
C64 |
220uF Why so large? |
Why are these components used? Do these additional components contribute to better output video quality? Which EVM is correct?
And does
1. OPA357AIDBVRG4
2. OPA357AIDBVT
Require different power connection style, which caused the difference above?
I would like to have some recommendation on this DAC power connection. Could anyone provide any schematic or PCB file here?
Thanks,
Zheng