Other Parts Discussed in Thread: TIDA-01471, THS4551, XTR111, THS4561, THP210
Hi!
we are experimenting with predictive maintenance in the factory of our client, on lathe spindle bearings. The single axis accelerometer sensor we would like to use is CMSS 2100 from SKF. The datasheet here. What we would primarily do is spectral analysis at Fs=20kHz. We need to design an interface for signal conditioning with probably an external ADC. We found a promising design here. Since we are new on this field our first question is: can we use this design with the CMSS 2100 sensor? Or can you recommend us a similar design to start with?
If TIDA-01471 is suitable, would you recommend an alternate part for THS4551IRGTT and XTR111AIDGQT? They are unavailable at the moment and it seems like for a year, at least.
Thank you!