I am using the VCA810 for a gain control circuit. I have it in an AGC loop and it works well. As another option from my multipurpose board, I wish to drive the control input directly from a DAC and get linear gain which is not possible as the VCA is a logarithmic type gain. In my prototype I have already scaled and negated the output of the DAC (0->3V to -2->0) but did not take into account the VCA logarithmic output. Is there an interface circuit which can take the linear output of the DAC and transform it to get a linear gain control from the output of the VCA?