Part Number: DRV110EVM
Other Parts Discussed in Thread: DRV110
I'm using the DRV110EVM that I just received, and I am having a problem. There is a pot for R_HOLD, but no matter what position it is in, the hold current does not change, it stays at 140 mA. When I turn the pot for R_Peak, the peak current is adjusted appropriately.
I've measured the resistance at pin 4 on the part to ground and it does match the resistance measured at the test point next to the resistor. So the hardware does seem in good working condition as far as I can tell
I will note that I did turn the pot all the way up to 1M at one point, and afterwards I noticed the spec sheet says that resistance should be less than 333k.
Am I doing something wrong to adjust the hold current?
Thanks,
Matt