Part Number: LM324LV
Other Parts Discussed in Thread: LMV324A, LMV324, LMV324-N, TINA-TI, TLV9004
Hello team,
I have question about full swing output voltage with open-loop.
The our evaluated schematics is using V+=5V,V-=GND, Load =about 20Kohm. It used as comparator.
if IN+>IN-, I expected output voltage is lower 1V than V+ based on claw graph , however actual output voltage was almost 5V.
Does the LM324LV have output rail to rail function?
Best regards,
Sato