Part Number: INA326
Hi Team,
I tried to simulate INA326 with current source input.
I get convergence error for Transient analysis- Calculate operatingpoint/zero initial values/use initial condition option.

Kindly suggest.
Regards,
Vidhya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA326
Hi Team,
I tried to simulate INA326 with current source input.
I get convergence error for Transient analysis- Calculate operatingpoint/zero initial values/use initial condition option.

Kindly suggest.
Regards,
Vidhya
Hi Vidhya,
Thanks for your post. Can you please attach your TINA file? I'd like to open it and take a closer look at the issue here.
Hi Vidhya,
you set the gain of INA326 to 2 x 160k / 2k = 160,

but at the same time you heavily overdrive the input if INA326:

This cannot work.
Why is R4 so high??
Kai
Hello Kai,
I tried to add noise filters.
Do we need to add the noise filters - R4,R5, C6,C7 and C8 as highlighted below? How to decide those values?
Please suggest.
Also share the working .tsc

Thanks and Regards,
Vidhya
Hi Vidhya,
if this was the plan, then you have omitted the second 10k resistor and you have erroneously mounted the 10k resistor within the 100µA constant current path.
Yes, using the input filter is mandatory when handling very small signals and if they come from the outer world.
Kai
Hi Kai,
How to calculate the filter values?
I tried to simulate now without input filters, but output 5734.ADC sim.TSCshows <10mV range instead of 2.9V for which the gain is set.
RTD=177.23Ohm, Expected output is 2.91V but the value read is 6.08mV.
VM3 voltage is as expected- 17.72mV.

PFA .tsc file.
Kindly share your thoughts.
Thanks,
Vidhya
Thanks Kai,
But VF1 has reached 603.91mV for 177 Ohms.
The gain is set to 160 to reach this VF1 to 2.84V (for a 3V full scale)
Why is the VF1 read as 603mV?
KIndly clarify.
Thanks,
Vidhya
Hi Vidhya,
100µ x ((177 +10) - (78.7 +10)) x 160k / 2k x 2 x V = 1.57V which exactly equals the voltage at the measuring point VP_8. So the circuit is working well.
Kai
Thanks Kai.
Gain is set to 160. So vout at 177 ohm is expected to be 2.9V. But simulation shows 1.57V
Please clarify how to overcome this offset.
Regards,
Vidhya
Hi Vidhya,
You could increase the gain from 160V/V to 295V/V. See attached and confirm.