This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP7704: LMP7044 Input Current Noise vs Frequency

Part Number: LMP7704

Hello!

I was wondering if there was any additional information about the noise density of the LMP7704 at lower frequencies. I'm interested in using this amplifier in a lower bandwidth application where the 1/f noise could become an issue. I was wondering if there was a graph that could be provided similar to the input voltage noise density vs frequency? If a graph is not available, is there any information on the current noise density at frequencies lower than 100kHz

Thanks,

Billy