This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Current to frequency solution-High accuracy



Hi team,

Is there any solution that can convert mA level current to voltage output with high accuracy? Below is the input range and accuracy requirement. 

Input: -30mA~30mA

Voltage output

Accuracy: 10ppm.

Thank you!

Best regards

Yunjing