Part Number: OPA2387
Other Parts Discussed in Thread: OPA387,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA2387
Other Parts Discussed in Thread: OPA387,
I am confused by the definition of the offset voltage in the datasheet.
Under which conditions is the maximum 1 (first line) / 1.5(second line) / 2µV(other lines)?
The default test conditions are listed above the table. The "test conditions" column specifies how the test conditions for this line differ from the default.
But does this make sense?
Over the whole temperature range (first line) it is 1µV, and else (when?? Third line) it is 2µV?
I still don't get it.