Part Number: INA281-Q1
Other Parts Discussed in Thread: INA281
Hi team,
My customer evaluated INA281A2QDBVRQ1 in their project, and met some issues now. Could you please kindly help to give some suggestions?
Refer the datasheet, INA281A2QDBVRQ1 can normally work as long as the output voltage is below VCC-0.3.
But they found the IC won't work properly when it output 2V at high temperature(105°C).
Then at the normal temperature, the IC can work well.
The VCC is 3.3V. Rs is 0.002ohm.
Below is the test result and schematic.
Thanks for your help.
Regards,
Ivy
The blue curve is output voltage, green curve is output current.