Other Parts Discussed in Thread: THS6012, THS6022, BUF634A, LME49724, TINA-TI, THS4151, THS4150, THS4552
Hi, I am looking for a balanced output amplifier of a signal generator 0 - 300kHz, Vcc +/-16V, output total Rload 200R (between + and - output), Vout +/-14Vmax (+/-56Vpp), gain 3-4V/V, mostly resistive load. The most likely circuit would be composite with an appropriate signal opamp at the front. The main performance criteria are THD+N and IMD.
Please which of your high-speed high-power opamps would you recommend? Could THS6222 offer lower THD+N/IMD than the older THS6012?
THS6222 datasheet shows a huge increase in IMD for frequencies below 1MHz. Is that the case with THS6012 too? Is there a way to avoid the IMD increase in THS6222 using the composite connection with another high-gain front opamp? TPA6120 (sibling of THS6012 IIUC) componsite circuits feature very low IMDs at <1MHz.
THS6222 datasheet HD2/3 charts start at 1MHz. The gain charts start at 5V/V, is the device stable at gain 3-4V/V? According to the datasheet TPA6120 allows gain 1V/V.
Thank you very much for your help.
Best regards,
Pavel.