Part Number: INA301
Hi,
I tried to simulate INA301A1 model using TINA. I see error values at the output waveform.
Model file and screenshot attached
Input power supply voltage, V2: 5V
Load current, IG1 = 2A STEP
I see in the waveform,.
- IG1 as 3A, (expected 2A)
- OUT_A1 as 5V (expected 4V)
- VIN_A1_DIFF as 300mV (expected 200mV)
.