Part Number: AMC3302
Other Parts Discussed in Thread: AMC3330
Hello, I have a problem with the design of a current and voltage sensor based on the AMC3300 and AMC3302 ICs. It is about DC sensing in a battery operated high voltage system.The AMC3302 circuit is used to sense the current using voltage drop across a 100 micro Ohm measuring resistor. Unfortunately, I am unable to get a zero value when the load is disconnected, I get a voltage of around 25 micro volts at the output of the AMC3302 and I cannot get a zero at the connected ADC.The AMC3302 circuit is used to sense the current using voltage drop across a 100 micro Ohm measuring resistor. Unfortunately, I am unable to get a zero value when the load is disconnected, I get a voltage of around 25 micro volts at the output of the AMC3302 and I cannot get a zero at the connected ADC. The device requires sensing even very small currents, I can't use a dead band around zero.
For the AMC3300 circuit, the voltage results are without problems
Do you have any advice or idea please?
Best regards
Matej