Part Number: OPA2182
Other Parts Discussed in Thread: OPA211
Hi Team,
customer is selecting the right component for an industrial application design.
he found that OPA2182 is an component with certain required features but regarding the CMRR/PSRR at high frequency the component is not matching my requirements.
He'd like to know if TI has fabricated similar component but with enough CMRR/PSRR at 300Mhz.
I researched the datasheet and find most of CMRR/PSRR are at Max 10MHz freq.
I can only find OPA211 series have Max freq. range 100MHz for CMRR parameter after I checked lots of op amps.
Now, could you be son kind as to let me know the electronics components (op amps, instrumental amplifier, etc.)
with the highest CMRR/PSRR at high frequencies in TI catalog (does not matter the number of channels or other parameters).
It would be a great help for me to have an official answer from TI so I could re-focus and try to meet the technical requirement of my design in a different way.

Thanks.