This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA260: I2C scanning problems

Part Number: INA260

Hi I have a controller cards with 8 INA260 (I260AI 05KG4 A1YD) that have been working flawlessly, but now I have got a new batch of cards (I260AI 07KG4 CPG8) this one are not responding correctly when I use I2C scanner. Addresses used are 0x40 to 0x47 and everything is fine when I scan the old one and I also get the correct response when reading the data, but with the new one only 0x44 to 0x47 show up during scan and then when I try to read data from this four addresses  I get an error like it is not the correct IC. Any idea what could be wrong?