Part Number: LM139A
Other Parts Discussed in Thread: LM339, LM139
With a negative input of -12V through 3K Ohms, we've never experienced a false state but are we "on the edge"? Opposite input = +1.2V through 750 Ohms.. Operation at +15 to +30C. The datasheet states that "input current flows through parasitic diode to ground and will turn on parasitic transistors that may increase Icc and may cause output to be incorrect". I would have added a clamp diode but the design has been in use for 20+ years so overall enthusiasm for adding a diode now is rather less than non-existent.
"May cause the output to be incorrect". And, obviously, may not. But under what circumstances specifically? It appears that at least some of the current would flow through the forward biased input transistor collector-base junction to ground. Is this path more predominant than the parasitic diode?
Thanks