Other Parts Discussed in Thread: DRV2700EVM, DRV2700EVM-HV500, DRV2700
We did test your DRV2700EVM-HV500 and DRV2700EVM with our EAP type haptic actuator, with capacitance over 200nF and which should be driven at 212 Vpp (0 – 212V) with frequencies up to 150Hz.
By using the DRV2700EVM-HV500 we’re limited to 50% of duty-cycle at 20 Hz (see attached image).
Is it possible to use the DRV2700EVM IC on the evaluation board to drive the actuator in higher frequencies and duty-cycle? Maybe by changing some of the components present on the Evaluation board?
Thank you for your support