This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2830: Very basic question about the usage of "beffer" amp

Part Number: OPA2830

Hi,

Let me study about the usage of OPA2830 as a buffer.

Please check the attached file.

I made the buffer amp by using OPA2830 and evaluated it.

The condition is as below.

  Vs=+/-5V. Vin=1Vpp, 1MHz sinwave, Rf=10ohm, Rin=1Kohm

In this condition, the amp worked well.

But in case of Rin=0ohm, the output signal seems to noisy and a little bit unstable, I felt...

My question is, do I need Rin or Rf (or both) for OPA2830 to use?

And will you give me the phase margin of OPA2830?

Thank you for your support.

Best Regards,

Takumi

OPA2830 Buffer.pdf