Other Parts Discussed in Thread: PGA280, LMH6401, THS7530, VCA2612, VCA2617, LMH6514, VCA2615, VCA820, PGA870, THS4561, VCA810
Hello,
I am looking for a PGA/VGA with a ac-coupled bipolar input swing. I have looked through the parts available and found a couple of options like THS7530, LMH6401 and PGA280.
The required specs are : Fully differential amplifier with output swing in the range of +/-2.5V and gain of -20dB/0dB to 60dB and frequency range of operation is 100kHz max.
The problems with the parts I found is as follows:
THS7530 - min gain of 11dB, required minimum gain is 0dB and better if some -10dB attenuation is a option
LMH6401 - very high bandwidth and none of the response plots cover the required frequency range and high bandwidth noise may be also an issue
PGA280 - noise figures are very high
If I have overlooked any parts which work out for the application, please suggest.
Any suggestion to achieve the required programmable gain will be a great help.