Other Parts Discussed in Thread: LM317, OPA567
Dear Team,
I need an opamp with 1A output current(max) for my circuit.
The opamp will be used as a unity gain buffer. Could you please suggest one. Below is my circuit.

Regards
HARI
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can you give more information about your application? Like output range, frequency, SNR, load or someting.
Thanks!
See the list of power op amps: www.ti.com/amplifier-circuit/op-amps/power/products.html#p480=1;1&p233typ=1000;10000
What is the supply voltage, i.e, how much power do you need to dissipate inside the device (1 A * VCC/2)? Most devices will have a problem with a DC current of 1 A, and are likely to require active cooling.
Hello Hari,
If output current always flows out of the op amp, add an NPN or NMOS transistor

For VOUT = VIN + 1.25V , try LM317
If you need something else, what is the voltage for VIN and U1 power?
Hari,
If output current only flows one way then the transistor will boost the current. If you need bidirectional output current then a different solution will be needed.
OPA567 is an option.