Part Number: THS4531
Hello,
We had a THS4531 damaged during our circuit card test.
Our THS4531 is powered from 5V and has a common-mode setpoint of 2.5V. Its output is connected to an ADC through 100 Ohm (each leg) and 2nF at ADC input.
The THS4531 failure symptoms are as follows :
1) Both outputs of THS4531 are stuck near 0V.
2) Both outputs of THS4531 show a very small impedance (~5 Ohm) to Vs-.
It is possible that the THS4531 outputs have been shorted together or to GND during our circuit card test.
My question :
From the datasheet, it appears that the THS4531 outputs are not short-circuit protected. Should I expect damage from shorting the outputs together or outputs to GND ?
Thank you
Louis Gagnon