Part Number: OPA818
Hello,
I was simulating an amplifier circuit with OPA818. I'm using two of them with each 10 x gain to achieve 100 x amplification. My input voltage is between 0.001 V and 0.035 V. I did everything according to the data sheet of the op amp, but amplification is not 100. depends on the input voltage, amplification differs between 90 and 140. I'm using LTspice and the model of OPA818, which I downloaded from the TI product website.
This is my circuit.

Many thanks in advance.
Ali