Other Parts Discussed in Thread: INA331, INA818, INA121, INA332, , LMP7721, TINA-TI
Hello all,
I am in the process of developing a circuit to measure the device current, the minimum device current in the order of picoamp. The shunt resistor is fixed to 50 Ohm, and I don’t have any flexibility in changing the shunt resistor. The measurement is from the low side, making my common-mode voltage to be nearly zero. The following are my requirements
- Low side current sensing
- Vcm=0V
- pA current measurement
- unidirectional current measurement
- analogue voltage output
Bandwidth and slew rate is not a constraint as I am interested only in the steady-state results.
The instrumentation amplifier should have a bias current of 10fA to measure 1pA current reliably with an accuracy of 99%. On searching the list of available instrumentation amplifiers meeting the above requirements, I find only offering from bias currents of the 20pA, making the minimum measurement limit to 2nA. The following are the top3 in my list
INA111, INA121, INA818 (with Vs up to 36V support). INA331/321 and INA332 were good too and are single rail supply designs. So with this, I have the following questions
- What are all the instrumentation amplifier choices for the above requirements?
- Instrumentation amplifier offers parasitic resistance rejections, which opamps don’t show, but specific opamps have lower input bias currents. So should I prefer opamps over ins-amps, or should I stick with ins-amps?
- Any other constructive suggestions or views I should incorporate?
Thanks
SK