Part Number: INA228
I am experiencing an offset to expected current readings and am having difficulty understanding where they may be introduced from. With current from -10A to +10A, the offset is consistently around -200mA. The amplifier is being used in a low side measurement configuration on a 500A battery shunt. The traces are about 1 inch each to the kelvin connections on the battery shunt (between GND and Shunt Load on Schematic)
Shunt resistor = 0.1 mΩ
SHUNT_CAL = 1280
VBus = 12V
Schematic:

Any insight as to where this offset may be coming from would be much appreciated!