Part Number: OPA2205
Other Parts Discussed in Thread: OPA192
Hi,
I created difference amplifier of gain 7.5.
Input voltage is 335mV. But, I'm getting output voltage of 7.55V. Expected output voltage was 2.51V,
What is root cause of this error?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The root cause is that you violate the common mode voltage requirements in OPA2205. For a single supply voltage, the Vcm needs to be above 1Vdc.

It would be ok if you use dual supply voltage rails as an example below.

If you have additional questions, please let me know.
Best,
Raymond
Thanks Raymond for prompt response,
I do not have negative power supply in my design.
I have replaced OPA2205 with OPA192 and added diode, capacitor circuit at the output of OPAMP.
Same error is not seen with OPA2205 when diode, capacitor and resistor (10K) added.
Hi Sadashiva,
The issue seems to be that particular schottky diode and 100nf capacitor. I changed to Si Diode and different schottky diodes, the convergence issue went away.
If you have to place 100nf capacitive load at the output, you may require to compensate the OPA192, so that the circuit can drive a capacitive load.

If you have additional questions, please let me know.
Best,
Raymond