Part Number: LF412-N
Hi,
Customer build a simple voltage follower (buffer) circuit using the LF412CN however they observe that the output hit compliance (Max Vcc Voltage) after they adjust the input voltage below 1V (all behavior is normal above 1V).
They want to know if this is normal or the device is defective. They encountered this in all the LF412CN batch.
Regards,
Maynard