Part Number: INA226-Q1
Other Parts Discussed in Thread: INA226
Hi sir,
I created the INA226 schematic by figure.21 in the datasheet and I used R filter=10 ohm, C filter=0.1uF.
If the Vbus=0.75V and current is 1A, the R shunt is 0.005 ohm and then the V shunt value is 5 mV ?
Is it right ?
How can I find the register value to verify the V shunt value ?
If the current is 500mA, then I need to adjust the R shunt value to 0.01 ohm to get the V shunt value is 5 mV?