The datasheet says that IC has
internal hystersis .Then how to give Upper threshold and lower threshold voltages to it? or Do we have to connect the resistors R1 and R2 EXTERNALLY? or are they internal in the IC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The datasheet says that IC has
internal hystersis .Then how to give Upper threshold and lower threshold voltages to it? or Do we have to connect the resistors R1 and R2 EXTERNALLY? or are they internal in the IC?
Clemens, thank you for your input.
Apoorva, as Clemens has mentioned, the internal hysteresis is already there and is not implemented without any extra resistors, so you can calculate your upper and lower threshold voltages from that internal hysteresis voltage. If you want more hysteresis, you can add the resistors and your threshold voltages will just include the internal hysteresis from the comparator and external hysteresis from the resistors.